McSPI controller peripheral example failures with some HW setups

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-9869
    • PROCESSOR_SDK_06_03_02_00
    • PROCESSOR_SDK_08.01.00
    • Hide
      am571x-idk
      am574x-idk
      am572x-idk
      Show
      am571x-idk am574x-idk am572x-idk

      McSPI master slave examples are not producing stable PASS results when repeated multiple times with different setups. All the tests run fine some times but errors are observed with different tests in different test conditions. Failures are attributed to the setup dependencies (cables used to connect the board).

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2974 - McSPI controller peripheral example...
                SYNCHRONIZED
                • Last Sync Date: