False test fail condition reported by diagnostic test framework

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Low
    • PDK
    • PDK-10276
    • PROCESSOR_SDK_06_03_02_00
    • PROCESSOR_SDK_08.01.00
    • Hide
      am572x-evm
      am571x-idk
      am574x-idk
      am572x-idk
      Show
      am572x-evm am571x-idk am574x-idk am572x-idk

      Diagnostic test framework is reporting false failure while running the GMAC and QSPI diagnostic tests even though test completes without any errors. Diagnostic test framework is executed from SD card. Tests are executing fine when run from CCS.

      Sample log for QSPI test is shown below

      *********************************************
      QSPI Test
      *********************************************

      Testing QSPI read/write...
      Test PASSED!
      Testing QSPI Sector Erase...
      Test Passed! ==> Test exits with PASS result

      Finished running qspi_TEST, result failed! ==> Diagnostic framework reports test as fail which is not correct

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2976 - False test fail condition reported ...
                SYNCHRONIZED
                • Last Sync Date: