"Execute selected reset after program load" setting does not appear to work

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium

      The "Execute selected reset after program load" setting does not appear to have any effect as the reset does not appear to occur after the program load. When manually pressing the "Reset Now" button, a message appears in the console indicating a reset occurred. No such message occurs when a program load is completed and the aforementioned setting is enabled. The target also does not behave like a reset occurred.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2969 - "Execute selected reset after progr...
                SYNCHRONIZED
                • Last Sync Date: