Load/Verification actions take no effect if CPU2 is flashed/verified before CPU1 on a multi-core device

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      On a multi(dual) core device, if load/verify actions are done first on the second CPU after UniFlash startup, then load/verify actions for the first CPU have no effect. It appears that actions are not even run as there is no console output indicating such. Actions on CPU2 will continue to work.

      If load/verify actions are done first on the first CPU, then it will work on both first CPU and second CPU.

      The issue was reproduced on an F28377D and F28379D. Any dual core program can be used.

      The issue has been reproduced on UniFlash 6.3.0 and UniFlash 5.3.1

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2965 - Load/Verification actions take no e...
                SYNCHRONIZED
                • Last Sync Date: