-
Type:
Bug
-
Resolution: Fixed
-
Priority:
High
-
SimpleLink CC13x2-26x2 SDK BLE5 Stack
-
BLE_AGAMA-3247
-
BLE Stack BLE5-2.2.1 RC12
-
-
CC26X2R1
Git \ Installer version:
- 5.10.00.48
Last successful Installer: - Unknown
Test-Bed: - eRPC node + provisioner (BlueZ/Android Phone)
Application: - The provisioner is either a BlueZ-5.58 or a nRF Mesh application
Problem reproducibility: - 100%.
Problem description: - When provisioning a node using input OOB, the provisioner shows a string/number that the user needs to input on the node.
- When doing so, after inputting the number/string the application isn't sending that data back to the provisioner as it should.
- This fails the provisioning process.
- Notes:
- The Issue applies for both PB-ADV & PB-GATT
- This doesn't happen with other OOB types (no/static/output OOB)
- When using nRF Mesh application with input OOB configured, there is an option to provision with no OOB. when running the process this way issue doesn't reproduce.
Steps to reproduce the issue:
- Notes:
- Configure eRPC mesh node with Input OOB & initiate provisioning process
Attachments: - Network Log showing the issue
- Node configuration JSON