Out of the box ble5stack examples fail to sustain a connection with blestack peripherals

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3214
    • BLE Stack BLE5-2.2.0 PR
    • Hide
      BLE Stack BLE5-2.2.2 RC1
      BLE Stack BLE5-2.2.2
      Show
      BLE Stack BLE5-2.2.2 RC1 BLE Stack BLE5-2.2.2
    • CC26X2R1

      A CC2652 device loaded with a BLE5 simple_central or multi_role out-of-the-box project fails to maintain a connection to a previously paired/bonded CC2640R2 BLE4 simple_peripheral

      The connection is maintained indefinitely when a new pair/bond is established. However, a disconnect followed by a re-connect re-uses the previous bond but issues a timeout (error 0x22 or LL_STATUS_ERROR_LL_TIMEOUT) after tens of seconds.
      This issue happens with all permutations of SDK4.30 and 4.40 for both CC2652 and CC2640R2. Also, this issue does not happen with BLE5 stack for CC2640R2.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2942 - Out of the box ble5stack examples f...
                SYNCHRONIZED
                • Last Sync Date: