icssg: RX ch teardown timed out observed in NIMU restart

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Ethernet Switch Firmware
    • ETHFW-1810
    • ETHFW_08_00_00
    • ETHFW_08_00_00
    • am654x-idk
    • NDK in maintenance mode, no update releases planned

      UDMA RX channel teardown time out observed when running NIMU restart test:

      Restarting the NDK/ENET, 1!
      ICSSG Dual MAC Test
      EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK
      PHY 0 is alive
      PHY 15 is alive
      Host MAC address: 70:ff:76:1d:92:c1
      [NIMU_NDK] ENET has been started successfully
      Icssg_handleLinkUp: icssg0-1: Port 1: Link up: 100-Mbps Full-Duplex
      ENET NIMU App: Added Network IP address I/F 1: 10.24.50.69
      ENET NIMU App: Removed Network IP address I/F 1: 10.24.50.69
      Unregister async IOCTL callback
      Unregister TX timestamp callback
      Icssg_handleLinkDown: icssg0-1: Port 1: Link down
      
      [UDMA] [Error] RX ch teardown timed out!!!
      EnetHostPortDma_close: Assertion @ Line: 175 in src/per/enet_hostport_udma.c: status == ENET_SOK

      This issue was observed in MII test, but it's not related to the MII interface type.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2903 - icssg: RX ch teardown timed out obs...
                SYNCHRONIZED
                • Last Sync Date: