can_profile_app not giving CAN TX signal output on J721E HS device

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • MCAL
    • MCAL-5205
    • Hide
      PROCESSOR-CORESDK_07.03.00
      PROCESSOR-CORESDK-SAFETY_07.03.00
      Show
      PROCESSOR-CORESDK_07.03.00 PROCESSOR-CORESDK-SAFETY_07.03.00
    • MCUSW_J7_01.06.00
    • j721e-evm

      can_profile_app (in TX-only, non-loopback mode) fails to boot (from OSPI boot mode) and send out signal on CAN-H (TX) line of first CAN when booted on J721E HS board.
      Not sure if can_profile_app has been tested on HS device yet.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2848 - can_profile_app not giving CAN TX s...
                ERROR
                • Last Sync Date: