Unexpected halt in Multi-Role when connected to multiple centrals

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-2981
    • BLE Stack BLE5-2.2.0 RC15
    • Hide
      BLE Stack BLE5-2.2.1 RC1
      BLE Stack BLE5-2.2.1
      Show
      BLE Stack BLE5-2.2.1 RC1 BLE Stack BLE5-2.2.1
    • CC26X2R1

      The issue occurs when the Master-1 script is running before the Master-2 script.
      After connection is established with the Master-1 the DUT sends L2CAP Connection Parameter Update Request. If the Master-2 connects and starts sending Connection Update Indication at this time – the DUT is stuck.
      Notes: the Master-1 script only establish connection to the DUT, while the Master-2 script after connection runs loops of Connection Update.
      The issue is not reproduced when the DUT runs the Simple_Peripheral app.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2836 - Unexpected halt in Multi-Role when ...
                SYNCHRONIZED
                • Last Sync Date: