Document how to specify floating point constants where lower half is zero for C2000 & CLA in user guide

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium

      Certain floating point operations on C28x CLA are shorter and faster if, in the case where one of the operands is a constant, the lower half of the constant, as expressed in float format, is zero. Therefore, supply the user with a way to indicate that the representation of a float constant should be the closest one where the lower half is zero.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2794 - Document how to specify floating po...
                SYNCHRONIZED
                • Last Sync Date: