c28 fpu64 swapff intrinsic error

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-7208
    • Hide
      C2000_18.12.0.LTS
      C2000_20.2.0.LTS
      Show
      C2000_18.12.0.LTS C2000_20.2.0.LTS
    • Hide
      C2000_20.2.5.LTS
      C2000_18.12.8.LTS
      C2000_21.6.0.LTS
      Show
      C2000_20.2.5.LTS C2000_18.12.8.LTS C2000_21.6.0.LTS
    • default
    • No workaround needed. An error is still generated, however, message is misleading.

      With fpu64 devices, using the __swapff intrinsic is outputting incorrect error message and should instead indicate that __swapff is not supported in fpu64 mode and to instead use __swapf.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2793 - c28 fpu64 swapff intrinsic error
                SYNCHRONIZED
                • Last Sync Date: