tiarmar.exe is denied permission to create an archive file on Windows 7

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-8639
    • ARMCLANG_1.2.0.STS
    • ARMCLANG_1.3.0.BETA1
    • default
    • Hide
      The tiarmar.exe file in the tiarmclang 1.2.0.STS installation can be replaced by the archiver from the tiarmclang 1.1.0+STS toolchain.

      Alternatively, you can use the TI proprietary Arm Code Generation Tools' archiver, armar.exe, to perform any archiving tasks.
      Show
      The tiarmar.exe file in the tiarmclang 1.2.0.STS installation can be replaced by the archiver from the tiarmclang 1.1.0+STS toolchain. Alternatively, you can use the TI proprietary Arm Code Generation Tools' archiver, armar.exe, to perform any archiving tasks.

      When the tiarmclang 1.2.0.STS toolchain's archiver, tiarmar.exe, is run on a Windows 7 machine, it is being denied permission to create an archive file.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2791 - tiarmar.exe is denied permission to...
                ERROR
                • Last Sync Date: