Request for 32b windows build of the host emulation libraries

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Won't Implement
    • Priority: Not Prioritized
    • Code Generation Tools
    • CODEGEN-8540
    • C7000_1.4.1.LTS
    • default
    • Hide
      C7x is designed for 64b architecture and use cases. The HE is designed with 64b feature in mind. Adding 32b feature is going to be a significant effort, as it has to be retrofit and is bound to pose several challenges. We cannot support this request because –

      32b HE is very Keyence specific need
      Adding this feature will cause delay to critical projects that has big impact on Sitara and Jacinto business
      Once the feature is added, there is good amount of recurrent cost and effort in maintaining the feature, for which there is no user other than Keyence.
      Show
      C7x is designed for 64b architecture and use cases. The HE is designed with 64b feature in mind. Adding 32b feature is going to be a significant effort, as it has to be retrofit and is bound to pose several challenges. We cannot support this request because – 32b HE is very Keyence specific need Adding this feature will cause delay to critical projects that has big impact on Sitara and Jacinto business Once the feature is added, there is good amount of recurrent cost and effort in maintaining the feature, for which there is no user other than Keyence.

      The library supplied with the Windows Host Emulation solution is built for 64-bit Windows, in release mode. The customer requests a variant built for 32b Windows.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2755 - Request for 32b windows build of th...
                SYNCHRONIZED
                • Last Sync Date: