Use of virtual functions causes many RTS print functions to be linked into the program

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      Inspection of the generated map file shows that there are a number of object files included from the runtime support library related to printing. The application does not call any print functions. The application does include some virtual functions. If the virtual functions are moved then the print related object files are also removed from the link.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2753 - Use of virtual functions causes man...
                ERROR
                • Last Sync Date: