Streaming address generator (SA) advance may be removed as dead code

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-8454
    • Hide
      C7000_1.4.0.LTS
      C7000_1.4.1.LTS
      Show
      C7000_1.4.0.LTS C7000_1.4.1.LTS
    • C7000_1.4.2.LTS
    • default

      If an instruction references the streaming address generator (SA) and advances it, but does not have a use of the instruction's result, then the entire instruction may be considered dead code and removed. If this occurs, generated code will be incorrect. This may occur when _SAnADV is called in C code, but the result is not used. For example: "_SA0ADV(float, NULL);"

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2702 - Streaming address generator (SA) ad...
                SYNCHRONIZED
                • Last Sync Date: