Misleading message occurs when importing a project with dependencies where the main and dependent project both reference the same dependent project

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium

      In cases where a main project has a dependency with two dependent projects and one of the two dependent projects also has a dependency on the other, an error message like the below can occur when importing the main project with the option to auto-import any dependent project found is enabled:

      This is because the project in question as already been imported by the main project, so when the first dependent project also tries to import the same project, it fails.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2744 - Misleading message occurs when impo...
                SYNCHRONIZED
                • Last Sync Date: