Sciclient RM IRQ fails when the input and output used is mapped in ROM

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-9005
    • PROCESSOR_SDK_07.01.00
    • PROCESSOR_SDK_07.02.00
    • am65xx-evm

      The Sciclient RM IRQ has a logic which checks if the input and output of an IR is mapped in the ROM table or not. The way the logic works is that at the Sciclient level the mapping is checked but not cleared. However, a flag which says the actual entries are cleared is set to true indicating it is cleared. This is fine if only one of the input or output is mapped.

      if both are mapped the logic in the Sciclient_rm_irq.c file fails to recognise the rom mapping for the output since a single flag which indicates the input is used is already set. This causes a confusion and the RM IRQ eventually fails.

      This was highlighted in https://e2e.ti.com/support/processors/f/791/t/908499

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2712 - Sciclient RM IRQ fails when the inp...
                SYNCHRONIZED
                • Last Sync Date: