Updating to EMU PACK 9.2.1.00042 cause verification errors on program load for some Hercules devices

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent

      When I update CCS to the latest available EMU Pack (9.2.1.00042), I get verification errors when trying to flash a program that had no issues before the update. This happens on a Hercules LAUNCHXL2-TMS57012. Interestingly I could not reproduce the issue on an LAUNCHXL2-RM46. One difference between the two is the endianness. The former is big while the latter is little.

      While the XDS110 firmware was updated to 3.0.0.14, i don't think the firmware on the probe is the issue. When I try to connect to the launchpad using a CCS version with an older version of the EMU pack, I don't get the error (even though the FW version remains the same).

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2681 - Updating to EMU PACK 9.2.1.00042 ca...
                ERROR
                • Last Sync Date: