'Sciclient_rmIrqRelease()' API is failing

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-8537
    • PROCESSOR_SDK_07.01.00
    • PROCESSOR_SDK_07.03.00
    • j721e-evm
    • Avoid using the Sciclient_rmIrqRelease API to release / re-route an interrupt already mapped to a MAIN R5F core.

      The Sciclient_rmIrqRelease API is returning -1. The parameters passed to this are matching with the corresponding Sciclient_rmIrqSet API. The irq release API is called in "MMCSD_Close" for a MMCSD regression test suite. Because of this, there is a failure with the subsequent re-open and so the next "MMCSD_open" that tries to re-map the same interrupt is failing.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2637 - 'Sciclient_rmIrqRelease()' API is f...
                SYNCHRONIZED
                • Last Sync Date: