CCS 10.x missing Windows registry entry which specifies the version number

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Low

      There is an issue with the Windows registry for CCS 10.x.

      1. the displayname value does no longer contain the version
        1. This means that when having more than one version installed (not that uncommon) the list under "App & features" in setting will just contain more entries with "code composer studio" but no chance to see what version it refers to.
      2. There is an obvious bug in theĀ "DisplayIcon" value it readsĀ "**unknown variable final_install_path**/doc/ccs.ico"
        1. This is most likely the cause of the icon in "Apps & Features" is a default windows icon icon for a program and not the CCS logo as is seen for older versions

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2550 - CCS 10.x missing Windows registry e...
                ERROR
                • Last Sync Date: