SPICC26XXDMA and SPICC26X2DMA drivers leave SPI peripheral enabled

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • TI Device Drivers
    • TIDRIVERS-4212
    • TIDRIVERS_4_30_01
    • TIDRIVERS_5_30_00
    • Hide
      CC13x2
      CC26x2
      Show
      CC13x2 CC26x2
    • The SPI driver leaves the SPI peripheral enabled between transactions. This makes it difficult to recover if an error occurs during a transaction. The SPI_cancel() API will now always disable the SPI peripheral.

      The SPI driver leaves the SPI peripheral enabled between transactions. This makes it difficult to recover if an error occurs during a transaction. The SPI_cancel() API will now always disable the SPI peripheral.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2518 - SPICC26XXDMA and SPICC26X2DMA drive...
                SYNCHRONIZED
                • Last Sync Date: