[EXT_SITMPUSW-27] gmake when run from windows command prompt with -j can sometimes lock up the command prompt Created: 11/Dec/24 Updated: 11/Dec/24 |
|
| Status: | Declined |
| Project: | Sitara MPU & SPMCU SDKs |
| Component/s: | None |
| Affects Version/s: | None |
| Fix Version/s: | None |
| Type: | Bug | Priority: | Not Prioritized |
| Reporter: | TI User | Assignee: | TI User |
| Resolution: | Unresolved | Votes: | 0 |
| Remaining Estimate: | Not Specified | ||
| Time Spent: | Not Specified | ||
| Original Estimate: | Not Specified | ||
| Internal ID: | SITSW-6144 |
| Found In Release: | 07.03.00 |
| Decline Reason: | This is a known issue in windows cmd prompt |
| Description |
|
This is a windows limitation. Workarounds,
This is not seen always. This issue is seen with library build only as well, so its not a sysconfig issue This isssue is not seen in Linux. This issue is not seen when using git bash for windows |