[EXT_EP-9639] Incorrect assert fires if SlNetIfNDK_recvFrom() is passed MSG_DONTWAIT Created: 10/Feb/20  Updated: 19/Feb/20  Resolved: 14/Feb/20
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
Product: Network Development Kit
Internal ID: NDK-469
Found In Release: NDK_3_60_00
Fix In Release: NDK_3_75_00

 Description   

See E2E post: https://e2e.ti.com/support/processors/f/791/t/834640#pi320966=3

NDK_recvfrom() will return an error if MSG_DONTWAIT is passed and no data is ready. SockRecv() is ultimately called in this path and that will exit with an error without filling in the sockaddr struct if MSG_DONTWAIT is used and no data is ready for the socket. 

SlNetIfNDK_recvFrom() checks the sockaddr struck BEFORE checking the return code of NDK_recvfrom(), and will thus cause an assert to be fired. 

SlNetIfNDK_recvFrom() should check the return value first, and return with an error if there is an issue. 


Generated at Sat Dec 13 11:32:49 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.