[EXT_EP-12242] Project wizard Example name input doesn't accept new name when using it for the second time Created: 14/Mar/25  Updated: 14/Mar/25

Status: Accepted
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Unresolved Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: Resource Explorer
Internal ID: REX-4025
Found In Release: REX_4.21.0
REX_4.20.0
Affected Platform/Device: Generic

 Description   

An error shows up when changing the name for an example before clicking create in Project Wizard after creating a different example and changing its name successfully.

It appears that the name input component is not updating properly, and not taking the new input inserted in the input field when the user tries to do that for the second time while using project wizard.


Generated at Sat Dec 13 11:39:10 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.