[EXT_EP-11457] Compiler hangs on compile-time access of non-zero indices Created: 14/Sep/23  Updated: 09/May/24  Resolved: 10/Oct/23
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
Internal ID: CODEGEN-11515
Forum URL: https://e2e.ti.com/support/sensors-group/sensors/f/1023/t/1270037
Found In Release: ARM_20.2.7.LTS
C2000_22.6.0.LTS
C6000_8.3.0
MSP430_20.2.0.LTS
C7000_2.1.0.LTS
PRU_2.3.0
C7000_3.1.0.LTS
MSP430_21.6.0.B1
C2000_21.6.0.B1
C2000_20.2.0.LTS
Fix In Release: MSP430_20.2.8.LTS*
C7000_2.1.3.LTS*
MSP430_21.6.2.LTS*
C7000_3.1.1.LTS
C2000_22.6.2.LTS*
C6000_8.3.13
ARM_20.2.8.LTS*
C2000_NEXT*
PRU_2.3.4*
C7000_4.1.0.LTS
C2000_21.6.2.LTS*
Affected Platform/Device: default
Release Notes: static_assert(x,y) examines x to determine whether it can be shown to be true at compile time. If x is an expression involving a variable, it must examine the definition of that variable to determine if it has a known value at compile time. If that variable is defined in terms of another variable, it too must be examined, and so on. If at any point in this chain of definitions one of the variables is a multi-dimensional array, the compiler will probably enter an infinite loop trying to evaluate the static assertion.

 Description   

This test case enters an infinite loop attempting to evaluate a static_assert involving an object ultimately initialized from a multi-dimensional array. static_assert(x,y) examines x to determine whether it can be shown to be true at compile time. If x is an expression involving a variable, it must examine the definition of that variable to determine if it has a known value at compile time. If that variable is defined in terms of another variable, it too must be examined, and so on. If at any point in this chain of definitions one of the variables is a multi-dimensional array, the compiler will probably enter an infinite loop trying to evaluate the static assertion.


Generated at Tue Apr 08 21:18:44 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.