[EXT_EP-11429] eDP to HDMI adaptors are failing Created: 11/Aug/23  Updated: 23/Apr/24  Resolved: 23/Apr/24

Status: Declined
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Duplicate Votes: 2
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: Processor SDK - Jacinto
Internal ID: ADASVISION-5955
Found In Release: PROCESSOR_SDK_09.00.00
Fix In Release: PROCESSOR_SDK_10.00.00
Affected Platform/Device: j721e-evm
j721s2-evm
j784s4-evm
Decline Reason: Duplicate of https://jira.itg.ti.com/browse/ADASVISION-6066

 Description   

eDP to HDMI adaptors are failing.  No error is seen during init, but nothing is displayed on the screen when using it

The ethfw is turned off as needed here, but the issue still remains across all SoC's.

This could be a sysfw delta from 8.6 to 9.0, as this was working in 8.6


Generated at Mon Apr 14 07:46:17 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.