MMCSD_write & MMCSD_read function fails for the numBlocks greater than 0xFFFF

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SITSW-6263
    • 10.01.00
    • 11.00.00
    • Hide
      am62xx-sk
      am62xx-sk-lp
      am62x-sip-sk
      am62a-sk
      am62p-sk
      am62d-evm
      Show
      am62xx-sk am62xx-sk-lp am62x-sip-sk am62a-sk am62p-sk am62d-evm

      The MMCSD_RAW_IO example by default tests the MMCSD_read & MMCSD_write for the buffer size 0x400000 (#blocks = 0x2000).

      If the buffer size is increased to, let's say, 0x2000000 (#blocks = 10000) then the MMCSD_RAW_IO example fails with the following logs:

      [MMCSD RAW IO] Starting...
      ASSERT: 0.763242s: ../../../mmcsd_raw_io.c:mmcsd_raw_io_main:65: status == SystemP_SUCCESS failed !!! 

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5297 - MMCSD_write & MMCSD_read function f...
                SYNCHRONIZED
                • Last Sync Date: