DPL - configure HwiP_MAX_INTERRUPTS based on SOC supported values

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Not Prioritized
    • SITSW-5005
    • 09.00.00
    • 11.01.00
    • Hide
      am243x-evm
      am243x-lp
      am64xx-evm
      Show
      am243x-evm am243x-lp am64xx-evm

      Currently, the HwiP_MAX_INTERRUPTS is set to superset value of 512 but based on device it could be lesser. 

      Instead of setting a superset value, it should be derived from SOC config to save memory.

      (7) AM2634: SDK HwiP_MAX_INTERRUPTS is set to 512 but AM2634 can only have up to 196 interrupts per core - Tesla EP Sitara MCU Forum - Tesla - EP - TI E2E support forums

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-5304 - DPL - configure HwiP_MAX_INTERRUPTS...
                SYNCHRONIZED
                • Last Sync Date: