UART DMA LLD SysConfig generates incorrect files

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-6492
    • 10.01.00
    • 11.00.00
    • Hide
      am243x-evm
      am64xx-evm
      Show
      am243x-evm am64xx-evm

      SoC tested on: AM64x & AM243x

      How to reproduce:

      1. In the CCS, import the example named uart_echo_dma_lld
      2. Once imported, open example.syscfg and go the UART section
      3. Add one more UART peripheral, and then go ahead and select the SDK Infra-> LLD and Transfer Mode-> DMA Mode
      4. Build the application, and one will run into the following error

       

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5140 - UART DMA LLD SysConfig generates in...
                SYNCHRONIZED
                • Last Sync Date: