Debug unlock certificate generation script does not generate DER certificate blob

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-7832
    • 11.01.00
    • 11.02.00
    • Hide
      am62a-sk
      am62p-sk
      Show
      am62a-sk am62p-sk

      The debug unlock certificate generation script in the SDK generates only the hex file and deletes the DER blob treating it as temporary file.

      ❯ python3 debug_unlock_x509_cert_gen.py -s am62px
      Generating debug certificate for am62px ...
      Debug unlock certificate created at ./soc/am62px/debug_unlock_cert_hex.h
      ❯ tree
      .
      ├── debug_unlock_x509_cert_gen.py
      └── soc
          ├── am62ax
          │   └── debug_unlock_cert_hex.h
          └── am62px
              └── debug_unlock_cert_hex.h 

      This is sufficient for those who are using TISCI message for JTAG unlocking.

      However, the TIFS supports JTAG unlocking via the CCS as well in which case the DER certificate blob is required.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6219 - Debug unlock certificate generation...
                SYNCHRONIZED
                • Last Sync Date: