Incorrect address size for I2C EEPROM

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-7136
    • 11.00.00
    • 11.02.00
    • Hide
      am243x-evm
      am243x-lp
      am64xx-evm
      am64xx-sk
      Show
      am243x-evm am243x-lp am64xx-evm am64xx-sk

      Example of I2C Driver for U33 (AT24C512C-MAHM-T)  is not correct (Addr = 0x51). This device is having 3 address pins (A2-A0).

      However the board.c file defines only 2 address lines (#define EEPROM_ADDR_SIZE  (2U)).

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6213 - Incorrect address size for I2C EEPROM
                SYNCHRONIZED
                • Last Sync Date: