MMCSD field Card Type is not ordered logically in the Sysconfig

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-7804
    • 11.01.00
    • 12.01.00
    • Hide
      am62xx-sk
      am62xx-sk-lp
      am62x-sip-sk
      am62a-sk
      am62p-sk
      am62d-evm
      am275x-evm
      am273x-evm
      Show
      am62xx-sk am62xx-sk-lp am62x-sip-sk am62a-sk am62p-sk am62d-evm am275x-evm am273x-evm

      This is the ordering of the different fields for MMCSD

      The "Card Type" field, which allows to select EMMC or SD, comes after the operating mode and clock frequency.

      This is not logical as the operating mode is chosen according to the card type so the later should come before the former.

      The correct ordering should be:

      • Select the MMC port.
      • Select the Card Type.
      • Select the operating mode.
      • Set the input frequency.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6192 - MMCSD field Card Type is not ordere...
                ERROR
                • Last Sync Date: