"sbl_uart_uniflash_stage2" is not prebuilt

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-6468
    • 10.01.00
    • 11.02.00
    • Hide
      am62xx-sk
      am62xx-sk-lp
      am62x-sip-sk
      am62a-sk
      am62p-sk
      am62d-evm
      Show
      am62xx-sk am62xx-sk-lp am62x-sip-sk am62a-sk am62p-sk am62d-evm

      AM62Ax MCU+SDK  "default_sbl_null_hs_fs.cfg" scripts has below step: 
      --file=../../examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62ax-sk/r5fss0-0_nortos/ti-arm-clang/sbl_uart_uniflash_stage2.release.appimage.hs_fs --operation=flash --flash-offset=0x0
       
      This "sbl_uart_uniflash_stage2.release.appimage.hs_fs" is not by default built in sbl_pre-built folder.
       
      Should we add it in sbl_prebuilt folder?. If not, then, should documentation be updated to add extra step of building this binary?
       
      AM62Ax MCU+ SDK: EVM Setup
       
       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6185 - "sbl_uart_uniflash_stage2" is not p...
                SYNCHRONIZED
                • Last Sync Date: