-
Type:
Bug
-
Resolution: Fixed
-
Priority:
Medium
-
SITSW-8456
-
11.01.00
-
11.02.00
-
The `gAppimage` variable, used in the SBLs as a scratch buffer for authentication and loading of the image, is intended to be allocated to the `.bss.app` section defined in the linker command files.
However, the following files allocate `gAppimage` to section `.app` which is different from the section `.bss.app`.
❯ rg -l "gAppimage.*section.*\".app\""
examples/hello_world/am62dx-evm/r5fss0-0_freertos/main.c
test/drivers/boot/sbl_ospi_linux_multistage_ddr_ecc/sbl_ospi_linux_stage1/am62px-sk/wkup-r5fss0-0_nortos/main.c
test/drivers/boot/sbl_emmc_linux_multistage_falcon_mode/am62px/sbl_emmc_linux_stage2.c
examples/drivers/boot/sbl_emmc_multistage/sbl_emmc_stage1/am62dx-evm/r5fss0-0_nortos/main.c
examples/drivers/boot/sbl_emmc_multistage/sbl_emmc_stage2/am62dx-evm/r5fss0-0_freertos/main.c
examples/drivers/boot/sbl_null/j722s-evm/wkup-r5fss0-0_nortos/main.c
examples/drivers/boot/common/soc/am62dx/sbl_ospi_stage2.c
examples/drivers/boot/common/soc/am62dx/sbl_emmc_stage2.c
examples/drivers/boot/common/soc/am62px/sbl_ospi_linux_stage2.c
examples/drivers/boot/common/soc/am62px/sbl_emmc_linux_stage2.c
examples/drivers/safety/reset_isolation/am62dx-evm/r5fss0-0_freertos/main.c
examples/drivers/boot/sbl_ospi_multistage/sbl_ospi_stage1/am62dx-evm/r5fss0-0_nortos/main.c
examples/drivers/boot/sbl_ospi_multistage/sbl_ospi_stage2/am62dx-evm/r5fss0-0_freertos/main.c
examples/drivers/ipc/ipc_notify_echo/am62dx-evm/r5fss0-0_freertos/main.c
examples/drivers/ipc/ipc_rpmsg_echo/am62dx-evm/r5fss0-0_freertos/main.c
The allocation in the default SBLs work just because of the linker internal logic.
If the following patch is applied that reduces the memory region by 1MB where the `.bss.app` is mapped
diff --git a/examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/linker.cmd b/examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/linker.cmd
index 90afe7352..94b501770 100644
--- a/examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/linker.cmd
+++ b/examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/linker.cmd
@@ -162,5 +162,5 @@ MEMORY
DDR : ORIGIN = 0x9CAA0000 LENGTH = 0x1B68000
/* This section is used by the SBL to temporarily load the appimage for authentication */
- APPIMAGE : ORIGIN = 0x84000000 , LENGTH = 0x1900000
+ APPIMAGE : ORIGIN = 0x84000000 , LENGTH = 0x1800000
}
one would expect the linker to throw the error as the `gAppimage` cannot anymore fit in the APPIMAGE. However, it does not throw an error and allocates the `gAppimage` to wherever it could find the required memory as shown
❯ rg gAppimage -- ./examples/drivers/boot/sbl_emmc_linux_multistage/sbl_emmc_linux_stage2/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/sbl_emmc_linux_stage2.release.map 3507:9cafb000 gAppimage 5111:9cafb000 gAppimage
If the following patch is applied which allocated `gAppimage` to `.bss.app`
diff --git a/examples/drivers/boot/common/soc/am62px/sbl_emmc_linux_stage2.c b/examples/drivers/boot/common/soc/am62px/sbl_emmc_linux_stage2.c index 115134010..51cee1ae8 100644 --- a/examples/drivers/boot/common/soc/am62px/sbl_emmc_linux_stage2.c +++ b/examples/drivers/boot/common/soc/am62px/sbl_emmc_linux_stage2.c @@ -54,7 +54,7 @@ * image authentication * The size of the buffer should be large enough to accomodate the appimage */ -uint8_t gAppimage[0x1900000] __attribute__ ((section (".app"), aligned (4096))); +uint8_t gAppimage[0x1900000] __attribute__ ((section (".bss.app"), aligned (4096))); uint32_t gImageSize = 0U; /* In this sample bootloader, we load appimages for RTOS/Baremetal and Linux at different offset
the linker expectedly throws the error
Linking: am62px:wkup-r5fss0-0:freertos:ti-arm-clang sbl_emmc_linux_stage2.release.out ... "linker.cmd", line 145: error: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section, or the section contains padded functions. run placement with alignment fails for section ".bss.app" size 0x1900000. Available memory ranges: APPIMAGE size: 0x1800000 unused: 0x1800000 max hole: 0x1800000 error: errors encountered during linking; "sbl_emmc_linux_stage2.release.out" not built tiarmclang: error: tiarmlnk command failed with exit code 1 (use -v to see invocation) make: *** [makefile:194: sbl_emmc_linux_stage2.release.out] Error 1