-
Type:
Bug
-
Resolution: Fixed
-
Priority:
Medium
-
SITSW-4872
-
09.02.01
-
12.00.00
-
The MMCSD_enableBootPartition sends the CMD6 to configure the EXTCSD register with the following arg
uint8_t bootPartition = ((bootAck << 6U) | (partitionNum << 3) | partitionNum); uint8_t bootBusWidth = 0x02; uint32_t arg = (uint32_t)((bootPartition << 8) | (0xB3 << 16) | (0x03 << 24));
This means, it configures the EXTCSD register as follows:
- Enable the Boot Acknowledgement flag.
- Change the boot partition, which ROM uses to boot from in eMMC alternate mode, to the passed partition number.
- Enable access to the passed partition number.
The first two configurations are completely independent of the last one. There can be a case where one wants to enable access to, let's say, BOOT1 partition but not wants to change the boot partition from which the ROM boots the SBL Stage1.