SysConfig does not generate correct FLASH section parameters.

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SITSW-7482
    • 11.00.00
    • 11.02.00
    • Hide
      am62xx-sk
      am62xx-sk-lp
      am62x-sip-sk
      am62a-sk
      am62p-sk
      am62d-evm
      am275x-evm
      am62l-evm
      Show
      am62xx-sk am62xx-sk-lp am62x-sip-sk am62a-sk am62p-sk am62d-evm am275x-evm am62l-evm

      Upon building an application like ospi_flash_io in the latest AM275 MCU PLUS SDK offering, the generated file from the SysConfig tool namely: ti_board_open_close.c is showing incorrect values when compared to the one input by the user in the SysConfig tool.

      1. Open SysConfig tool for ospi_flash_io.
      2. Change the parameters for FLASH > Jedec ID Read Configuration.
      3. Once done, build the application.
      4. Under ti_board_open_close.c, the values will be different compared to the ones set in SysConfig.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5734 - SysConfig does not generate correct...
                SYNCHRONIZED
                • Last Sync Date: