-
Type:
Bug
-
Resolution: Cannot Reproduce
-
Priority:
Not Prioritized
-
SITSW-7506
-
11.02.00
-
am243x-lp
-
Please refer comments
On AM243-LP MCU PLUS SDK, pick an example under: C:\ti\mcu_plus_sdk_am243x_INSTALL_PATH\examples\empty\am243x-lp\r5fss0-0_nortos\ti-arm-clang
- Add UART and have the configurations same as the AM243-EVM DMA LLD application.
- Upon building the application, the errors generated are:
Compiling: am243x:r5fss0-0:nortos:ti-arm-clang empty.debug.out: generated/ti_drivers_config.c C:/ti/ccs1270/ccs/tools/compiler/ti-cgt-armllvm_3.2.2.LTS/bin/tiarmclang -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mthumb -Wall -Werror -g -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -D_DEBUG_=1 -IC:/ti/ccs1270/ccs/tools/compiler/ti-cgt-armllvm_3.2.2.LTS/include/c -IC:/ti/mcu_plus_sdk_am243x_10_00_00_20/source -Igenerated -DSOC_AM243X -MMD -o obj/debug//ti_drivers_config.obj generated/ti_drivers_config.c generated/ti_drivers_config.c:45:27: error: use of undeclared identifier 'CONFIG_UART_NUM_INSTANCES' uint32_t gUartConfigNum = CONFIG_UART_NUM_INSTANCES; ^ generated/ti_drivers_config.c:47:25: error: use of undeclared identifier 'CONFIG_UART_NUM_INSTANCES' UART_Config gUartConfig[CONFIG_UART_NUM_INSTANCES] = ^ 2 errors generated. gmake: *** [makefile:153: ti_drivers_config.obj] Error 1
The issue is that gUartConfig and gUartConfigNum shows up in the generated map file but it is not supposed to be there. Internally the SysConfig uses the file: C:\ti\mcu_plus_sdk_am243x_INSTALL_PATH\source\sysconfig\drivers\.meta\uart\templates\uart_config_v0_lld.c.xdt
But in the map file the two variables defined above: gUartConfig and gUartConfigNum are named inside of C:\ti\mcu_plus_sdk_am243x_INSTALL_PATH\source\sysconfig\drivers\.meta\uart\templates\uart_config_v0.c.xdt