OSPI Phy Tuning Data is not written correctly in Flash_norOspiOpen()

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SITSW-6765
    • 10.01.00
    • 11.01.00
    • Hide
      am62xx-sk
      am62p-sk
      am243x-evm
      am243x-lp
      am64xx-evm
      am64xx-sk
      Show
      am62xx-sk am62p-sk am243x-evm am243x-lp am64xx-evm am64xx-sk

      Inside Flash_norOspiOpen API, we see that if the user fails to read the attack vector then we reflash the known buffer of 128 bytes to a known offset.

      But since we are using our entire SDK in Uniform mode of Flash, hence the way we rewrite the 128 bytes of data by doing a sector erase first will fail.

      The failure will happen as sector erase should not be implemented rather block erase should be written.

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-5728 - OSPI Phy Tuning Data is not written...
                SYNCHRONIZED
                • Last Sync Date: