FFT Magnitude graph should explicitly indicate the maximum FFT Order

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Graphs
    • DVT-1908
    • Hide
      CCS_7.1.0
       CCS_7.2.0
      Show
      CCS_7.1.0  CCS_7.2.0
    • CCS_8.0.0
    • N/A. Use a FFT Order lower than 16
    • Hide
      When inserting a FFT Order of 16 and above on the FFT Magnitude and FFT Magnitude and Phase, the plotted curve becomes corrupted.
      There is no warning about the maximum order, thus leaving to the user interpretation if this is a bug or a limitation.
      Therefore at this point:
      The calculation for orders larger than 15 should be fixed (if that was the original intent) and
      A small message should be displayed when the limit is reached
      Show
      When inserting a FFT Order of 16 and above on the FFT Magnitude and FFT Magnitude and Phase, the plotted curve becomes corrupted. There is no warning about the maximum order, thus leaving to the user interpretation if this is a bug or a limitation. Therefore at this point: The calculation for orders larger than 15 should be fixed (if that was the original intent) and A small message should be displayed when the limit is reached

      FFT Magnitude graph should explicitly indicate the maximum FFT Order

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-847 - FFT Magnitude graph should explicit...
                SYNCHRONIZED
                • Last Sync Date: