ET: Invalid response was received from the XDS110 error on Linux

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium

      The following error message will appear when running the target after ET is enabled on CCS Linux:

      Cortex_M4_0: JTAG Communication Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.7.0.00213)
      IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 9.7.0.00213)

      Issue was reproduce on Ubuntu 22.04 LTS with CCS 12.7.0 on a CC2652RB LaunchPad.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-4538 - ET: Invalid response was received f...
                SYNCHRONIZED
                • Last Sync Date: