[EXT_SITMPUSW-152] Heterogeneous-camera streaming with imx390 followed by ov2312 gets stalled. Created: 11/Aug/25  Updated: 11/Aug/25

Status: In Development
Project: Sitara MPU & SPMCU SDKs
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: High
Reporter: TI User Assignee: TI User
Resolution: Unresolved Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Internal ID: SITSW-4300
Found In Release: 09.01.00
Fix In Release: 11.01.00
Affected Platform/Device: am62a-sk

 Description   

When streaming from multiple cameras, a few problems have been observed. 

Two HW setups have been tested (please refer attached scripts for setup and streaming):

  • AM62A SK + Fusion Board + OV2312 (cam 0) + IMX390 (cam 1)

In SDK 9.1:

If the imx390 is streamed first, followed by streaming of ov2312, the ov2312 pipeline gets stuck.

Running both imx390 and ov2312 simultaneously is supported in SDK 9.2, but this issue persists in 9.2.

Fix details:
https://git.ti.com/cgit/processor-sdk/vision_apps/commit/?h=main&id=51dfdcd3081


Generated at Fri May 01 09:58:24 CDT 2026 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.