[EXT_EP-9633] TCP server sockets do not transition to listen state after call to listen() Created: 10/Feb/20  Updated: 19/Feb/20  Resolved: 11/Feb/20
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
Product: Network Development Kit
Internal ID: NDK-356
Found In Release: 1.71
Fix In Release: NDK_3_75_00

 Description   

The server socket in the tcpEcho example, while blocked on accept(), was showing "CLOSED". The expected state here is "LISTEN".

In the NDK stack, the transition to the "LISTEN" state doesn't happen until the listening socket receives a SYN request from a client. The if statement (that checks for a RX'd SYN) that encloses this state change also has a comment about the socket being in a listening state, although the code hasn't actually put it into that state yet:

Seems that the parent socket should have been put into the listening state during the listen call.


Generated at Sat Dec 13 11:34:45 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.