[EXT_EP-9510] C6000: callstack replicates caller function indefinitely when Step Into/Over Created: 26/Aug/19  Updated: 21/May/25

Status: Accepted
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Unresolved Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: Code Generation Tools
Internal ID: CODEGEN-6662
Forum URL: https://e2e.ti.com/support/processors/f/791/t/829800
Found In Release: C6000_8.3.0
Affected Platform/Device: default
Workaround: No practical workaround
Release Notes: The callstack mysteriously replicates the caller function indefinitely when stepping into or stepping over a function in C.

This was verified to happen with CCSv8.3.1 and v9.1.0 on Windows using CGT 8.3.3 for C6000.

 Description   

A function which does not return (such as one that contains an infinite loop) doesn't need to save the return address register, so the compiler may reuse it for some other purpose. When this happens, the debugger may show strange things, especially if the non-returning function itself calls a function, in which case the debugger will get confused and show in the call stack view an infinite recursion of the nested function, which is not correct. The bug is that the DWARF information wasn't updated to indicate that the return address register is invalid, which would have stopped the debugger from trying to interpret it.


Generated at Sat Dec 13 11:39:09 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.