[EXT_EP-9428] memory allocation functions do not robustly handle case of --heap_size=0 Created: 28/Jul/19  Updated: 25/Oct/23  Resolved: 28/Jul/19
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
Internal ID: CODEGEN-6501
Forum URL: https://e2e.ti.com/support/development_tools/compiler/f/343/t/579449
https://e2e.ti.com/support/development_tools/compiler/f/343/t/579454
https://e2e.ti.com/support/development_tools/compiler/f/343/t/579456
Found In Release: ARM_18.12.0.LTS
PRU_2.4.0*
MSP430_18.12.0.LTS
ARP32_1.1.0*
C2000_18.12.0.LTS
Fix In Release: C2000_18.12.4.LTS
ARM_18.12.4.LTS
PRU_2.4.0*
ARP32_1.1.0*
MSP430_18.12.4.LTS
Affected Platform/Device: default
Release Notes: It is possible to set the size of the allocation heap to a total size (such as zero) that is too small to handle any allocations. The C library's dynamic memory allocation routines (e.g. malloc) did not gracefully handle allocations in this case. These functions might crash, or might scribble on unrelated program memory, or might return successfully with a bogus pointer, in which case the caller would likely proceed to write through the bogus pointer and scribble on arbitrary memory.

 Description   

memory allocation functions do not robustly handle case of --heap_size=0


Generated at Sun Apr 13 14:36:59 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.