[EXT_EP-9418] switch statement where controlling expression is C++ scoped enum with underlying type smaller than int crashes compiler unle Created: 22/Jul/19  Updated: 19/Feb/20  Resolved: 22/Jul/19
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
Product: Code Generation Tools
Internal ID: CODEGEN-6476
Forum URL: https://e2e.ti.com/support/tools/ccs/f/81/t/822236
Found In Release: C6000_8.3.0
Fix In Release: C6000_8.3.5
Workaround: Doing any of the following will work around the bug:
- use any level of optimization from -O0 to -O3
- change the scoped enum to an unscoped enum
- specify the size of the enum as int or unsigned int
- change the switch to a tree of if/then/else statements
Release Notes: Compiling a C++ test case containing a switch statement where the condition is a scoped enum (a C++11 feature) with underlying t...

 Description   

switch statement where controlling expression is C++ scoped enum with underlying type smaller than int crashes compiler unle


Generated at Sat Dec 13 11:32:54 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.