[EXT_EP-9235] Compiler may lose volatile qualifier in A->B->C when B and C are both volatile Created: 14/Feb/19 Updated: 28/Mar/22 Resolved: 14/Feb/19 |
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
| Product: | Code Generation Tools |
| Internal ID: | CODEGEN-5943 |
| Forum URL: | https://e2e.ti.com/support/tools/ccs/f/81/t/770705 |
| Found In Release: | C6000_8.2.0 C2000_18.1.0.LTS C6000_8.3.0 ARM_18.12.0.LTS PRU_2.3.0 ARM_18.1.0.LTS MSP430_18.1.0.LTS C2000_19.6.0.STS ARM_16.9.0.LTS ARM_19.6.0.STS C7000_2.0.0.STS MSP430_18.12.0.LTS MSP430_19.6.0.STS C2000_18.12.0.LTS |
| Fix In Release: | MSP430_18.12.2.LTS ARM_18.1.6.LTS MSP430_18.1.6.LTS PRU_2.3.2 C2000_19.6.0.STS C2000_18.1.6.LTS C2000_18.12.2.LTS PRU_2.4.0* ARM_19.6.0.STS ARM_18.12.2.LTS C6000_8.3.4 C7000_2.0.0.STS C6000_8.2.7 MSP430_19.6.0.STS |
| Workaround: | The expression has to contain both dereferences, eg, a->b->c, for the problem to appear. If they're separated by using a temp, as in
T * volatile p; p = a->b; ... p->c ... then the problem should be avoided. Making the temp "p" volatile is also important, to prevent the compiler from recombining the two dereferences. Or compile with -o1, -o0, or -ooff. |
| Release Notes: | In an expression like A->B->C, when B and C are both volatile structure fields, we'd expect to see two distinct memory accesses every time. There is a bug in the compiler specifically with having two dereferences in a single expression, ie, A->B->C, in which it may lose the volatile qualifier from B. That may lead it to save A->B in a temporary variable and reuse that value instead of re-reading it as is supposed to happen. |
| Description |
|
Compiler may lose volatile qualifier in A->B->C when B and C are both volatile |