[EXT_EP-11936] Compiler incorrectly optimizes control flow code in the presence of an empty infinite loop Created: 05/Sep/24  Updated: 20/Mar/25  Resolved: 18/Feb/25

Status: Fixed
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Fixed Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: Code Generation Tools
Internal ID: CODEGEN-12833
Forum URL: https://e2e.ti.com/e2eprivate/figure-ai/figure-ai---ep/f/1295/t/1407343
Found In Release: ARMCLANG_3.2.0.LTS
Fix In Release: ARMCLANG_4.0.2.LTS
ARMCLANG_3.2.4.LTS*
Affected Platform/Device: default
Workaround: Workaround #1:

There is an empty while loop at the end of the function that contains the condition statement in question:

  while (true) ;

The 4.0.0.LTS compiler makes the assumption that this is a noreturn function and so the "if (!assert_fired)" condition check is optimized out.

To avoid having the "if (!assert_fired)" condition optimized away, insert an asm(" nop\n"); statement inside the while (true) loop at the end of the assertHandler() function in the test case source file.

   while (true) {
      asm(" nop\n");
   }

Workaround #2:

A more heavy-handed workaround is to apply an "optnone" attribute to the assertHandler() function like this:

__attribute__((optnone))
void Server::assertHandler(etl::string_view description, etl::string_view pretty_function,
                           etl::string_view file, uint32_t line)

 Description   

The attached file has a function that begins ...

void Server::assertHandler(etl::string_view description, etl::string_view pretty_function,
                           etl::string_view file, uint32_t line) {
  static bool assert_fired = false;

  // Protection from the infinite calling to the handler
  // if some of the code bellow triggers the assert.
  if (!assert_fired) {
    assert_fired = true;

Build it ...

% tiarmclang @options.txt file.cpp

Ignore the warning and note diagnostics.

Create the interlisted, demangled, disassembly with the command ...

% tiarmobjdump --demangle --source file.o > disassembly.txt

Inspect the disassembly to find the function begins ...

00000000 <figure::lib::logger::Server::assertHandler(etl::basic_string_view<char, etl::char_traits<char>>, etl::basic_string_view<char, etl::char_traits<char>>, etl::basic_string_view<char, etl::char_traits<char>>, unsigned int)>:
;                            etl::string_view file, uint32_t line) {
       0: b08c         	sub	sp, #48
;       : mbegin(begin_)
       2: f240 0700    	movw	r7, #0
;     assert_fired = true;

The static variable is assert_fired is assigned the value 1 without the conditional check that appears in the C++ source.


Generated at Fri May 01 10:05:08 CDT 2026 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.