[EXT_EP-11893] [Conformance test] Add format VX_DF_IMAGE_RGBX format to DSS M2M testcase Created: 12/Aug/24  Updated: 31/Oct/24

Status: Accepted
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Unresolved Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: OpenVX Framework
Internal ID: TIOVX-1713
Found In Release: 09.02.00
Fix In Release: 10.01.00
Affected Platform/Device: j721e-evm
j721s2-evm
j784s4-evm
j722s-evm
j742s2-evm

 Description   

There is a bug filed on PDK

PDK-14494 [DSS] FVID2_DF_RGBX24_8888 not supported in writeback pipeline - Texas Instruments JIRA (ti.com)

This could have been found earlier if we have this format VX_DF_IMAGE_RGBX tested as part of DSS_M2M conformance test.

VX_DF_IMAGE_RGBX  is mapped to FVID2_DF_RGBX24_8888  in display m2m target implementation, but FVID2_DF_RGBX24_8888 is not supported in driver.

So once this is fixed in the driver (i.e. above jira), please include this format in the testcase

TDA4VL-Q1: tiovx display m2m can't convert image to rgbx - Processors forum - Processors - TI E2E support forums


Generated at Fri Mar 14 08:43:18 CDT 2025 using Jira 9.12.17#9120017-sha1:aba4002bcd633f188b6a4bb5dd8a0e1f20b79ee4.