[EXT_EP-11471] Compiler fails with internal error "Bad kind: TYPE::type_pointed_to" Created: 06/Oct/23 Updated: 02/Apr/24 Resolved: 16/Oct/23 |
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
Internal ID: | CODEGEN-11634 |
Found In Release: | C6000_8.3.0 MSP430_20.2.0.LTS C7000_2.1.0.LTS C2000_22.6.1.LTS MSP430_21.6.0.LTS C2000_21.6.0.LTS PRU_2.3.0 C7000_3.1.0.LTS ARM_20.2.0.LTS |
Fix In Release: | MSP430_20.2.8.LTS* C7000_2.1.3.LTS* MSP430_21.6.2.LTS* C7000_3.1.1.LTS C2000_22.6.2.LTS* C6000_8.3.13 ARM_20.2.8.LTS* PRU_2.3.4* C2000_21.6.2.LTS* |
Affected Platform/Device: | default |
Workaround: | use --opt_level=0 or 1 instead of 2
See below for instructions on how to set compiler options per file instead of entire project in CCS projects: https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_project-management.html#file-specific-options |
Description |
With --opt_level=2, the optimizer generates "internal error" for arrays of pointers similar to below example: void foo(void) { char* argv[1]; parse_args(argv); }NOTE: earlier fix in CODEGEN-11223 missed a use case that this fix addresses. More details: static inline __erase_vector __parse_args(uint8_t* ptrInput, uint8_t* argv[]) { /* code here */ } Build it ... % cl2000 -@options.txt file.c "file.c", line 2639: warning #303-D: typedef name has already been declared (with same type) "file.c", line 2640: warning #303-D: typedef name has already been declared (with same type) "file.c", line 2679: warning #303-D: typedef name has already been declared (with same type) TP>> internal error: Bad kind: TYPE::type_pointed_to This is caused by a defect in the TI C/C++ Optimizer. TI Customer Support may be able to suggest a workaround to avoid this. Upgrading to the newest version of the compiler may fix this problem. Contact TI in the E2E support forums at http://e2e.ti.com under "Development Tools", "TI C/C++ Compiler". See the link titled "Submitting an issue". We need to see this ENTIRE error message and a complete, reproducible test case including ALL of the command-line options. Include the .pp file created by option --preproc_with_comment >> Compilation failure Replace that function with an extern declaration ... extern __erase_vector __parse_args(uint8_t* ptrInput, uint8_t* argv[]); ... and it builds clean. |