[EXT_EP-11227] Editing id in Annotations dialog box duplicates the number of rows in the table Created: 07/Jul/23  Updated: 14/Nov/23

Status: Accepted
Project: Embedded Software & Tools
Component/s: None
Affects Version/s: None
Fix Version/s: None

Type: Bug Priority: Medium
Reporter: TI User Assignee: TI User
Resolution: Unresolved Votes: 0
Remaining Estimate: Not Specified
Time Spent: Not Specified
Original Estimate: Not Specified

Product: Edge AI Studio
Internal ID: EDGEST-505
Found In Release: MC_1.0_Beta2
Fix In Release: MC_1.0_GA
Affected Platform/Device: None
Decline Reason: Cannot reproduce

 Description   

To reproduce:

  1. Create new project
  2. Import annotated dataset
  3. Go to 'Annotate' page, click on the '+' button to add/edit new labels
  4. Click on one of the id fields in the table, and try to enter an unused ID number. Hit enter.
  5. A new row appears with the new ID and a duplicate label name. 

Note that this is only a bug in the UI, the new ID does not get saved anywhere and does not appear after you refresh the page, or rename one of the labels.


Generated at Sat Dec 13 11:31:04 CST 2025 using Jira 10.3.7#10030007-sha1:a563685562f94d165eb4e158cfb2a142338d8c54.